|
(Read-Write) Set and query displayed data format of the NA mode measurement. |
|
|
Relevant Modes |
NA |
|
Parameters |
|
|
<char> |
Data format. Choose from: MLOGarithmic – Log magnitude MLINear – Linear magnitude SWR – Standing Wave Ratio PHASe - Phase in degrees. The trace wraps every 360 degrees, from +180 to –180 UPHase - Unwrapped phase in degrees. SMITh – Smith chart; series resistance and reactance. POLar - Magnitude and phase of the reflection coefficient. GDELay – Group delay (N9912A - S11 ONLY) ZMAG - Impedance, magnitude only. REAL - Resistive portion of the measured complex data. IMAGinary - Reactive portion of the measured data. |
|
Examples |
CALC:FORMat SWR |
|
Query Syntax |
CALCulate[:SELected]:FORMat? |
|
Return Type |
Character |
|
Default |
Depends on model and measurement. |
Last Modified:
|
22-Sep-2014 |
Added Real, imag, Zmag |
|
1-Aug-2011 |
Added unwrapped phase (A.05.50) |