CALCulate[:SELected]:MARKer<n>:FUNCtion:MINimum

(Write-Only) Causes the specified marker to find the lowest (minimum) amplitude of the trace.

For NA and CAT mode, this command operates on the selected trace. First select a trace using CALC:PAR<tr>:SELect.

Relevant Modes

CAT, NA, NF, PAA, SA, RTSA, Pulse Measurements,  FOPS

Note: SA & RTSA modes do NOT recognize the optional [:SELected] node.

Parameters

 

<n>

New or existing marker to move. Choose from 1 to 6.

Examples

CALC:MARK1:FUNC:MIN

Query Syntax

Not Applicable

Default

Not Applicable


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)

10-june-2016

Added RTSA mode (9.50)

21-Mar-2014

Added FOPS

29-Oct-2013

Added Pulse