CALCulate[:SELected]:MARKer:FUNCtion:PEXCursion <num>

(Read-Write) Set and query the excursion value. This is the vertical distance (dB) between the peak and the valleys on both sides. To be considered a peak for subsequent marker search commands, data values must "fall off" from the peak on both sides by the excursion value.

For NA and CAT mode, this command operates on the selected trace. First select a trace using CALC:PAR<tr>:SELect.

Peak Excursion and Threshold settings apply to all markers on each trace.

These settings remain through an instrument preset, but are reset to the default values when the FieldFox power is shutdown.

Relevant Modes

CAT, NA, NF, PAA, SA, RTSA, Pulse Measurements

Note: SA & RTSA modes do NOT recognize the optional [:SELected] node.

Parameters

 

<num>

Excursion value in dB.

Examples

CALC:MARK:FUNC:PEXC 3

Query Syntax

CALCulate[:SELected]:MARKer:FUNCtion:PEXCursion?

Return Type

Numeric

Default

0.5 dB


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)

10-june-2016

Added RTSA mode (9.50)

29-Oct-2013

Added Pulse