(Write-Only) Sets the FieldFox setting <char> to the location of the specified marker. For NA and CAT mode, this command operates on the selected trace. First select a trace using CALC:PAR<tr>:SELect. Note: SA mode does NOT recognize the optional [:SELected] node. |
|||||||||||||||||||
Relevant Modes |
The following <char> arguments are valid in each mode: An error is returned if <char> is not valid.
|
||||||||||||||||||
Parameters |
|
||||||||||||||||||
<n> |
Existing marker location from which <char> will be set. Choose from 1 to 6. |
||||||||||||||||||
<char> |
STARt - Sets the sweep Start value to the marker X-axis value. STOP- Sets the sweep Stop value to the marker X-axis value. CENTer - Sets the center frequency of the sweep to the marker X-axis value. DELay - Sets the electrical delay to that of the current marker group delay value. RLEVel - Sets the reference level value to the marker Y-axis value. TLFRequency - Sets the SA Mode Tune and Listen frequency to the marker X-axis value. |
||||||||||||||||||
Examples |
CALC:MARK1:SET CENT |
||||||||||||||||||
Query Syntax |
Not Applicable |
||||||||||||||||||
Default |
Not Applicable |
||||||||||||||||||
Last Modified:
01june2018 |
Added NF mode Opt. 356 (10.3) |
19-Oct-2010 |
Updated with DEL (5.30) |