CALCulate[:SELected]:MARKer<n>:TRACe <tnum>

(Read-Write) Moves an existing marker to the specified trace number. The marker and the CAT or NA trace must exist already. This feature is called Marker Trace in the User's Guide.

For NA and CAT mode, this command moves the selected trace. First select a trace using CALC:PAR<tr>:SELect.

Relevant Modes

CAT, NA, NF, PAA, SA, RTSA

Note: SA & RTSA modes do NOT recognize the optional [:SELected] node.

Parameters

 

<n>

Existing marker to assign to trace. Choose from 1 to 6.

<tnum>

Trace number. Choose from:

CAT, NA, and NF:

  • 0 - Auto. Marker resides on data trace when it is visible. Marker resides on memory trace when only IT is visible.

  • 1 - Data Trace

  • 2 - Memory Trace

SA:

  • 1, 2 ,3, 4

Examples

CALC:MARK1:TRAC 1

Query Syntax

CALCulate[:SELected]:MARKer<n>:TRACe?

Default

1


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)

10-june-2016

Added RTSA mode (9.50)