(Read-Write) Sets and queries the peak threshold value that defines the minimum signal level (or min threshold) that the peak identification algorithm uses to recognize a peak. |
|
Relevant Modes |
IQA (Spectrum only) |
Parameters |
|
<numeric> |
Minimum: -200 Maximum: 200 |
Couplings |
For a signal to be identified as a peak it must meet certain criteria: - Signals in the negative frequency range and signals very close to 0 Hz are ignored. - Signal must satisfy peak excursion (:CALC:SPEC:MARK:FUNC:PEXC) and peak threshold criteria before being identified as a peak. |
Examples |
CALC:SPEC:MARK:FUNC:PTHR -70 |
Query Syntax |
CALC:SPEC:MARK:FUNC:PTHR? |
Default |
-9.000E+01 |
Last Modified:
22oct2017 |
New IQA mode (10.1x) |