:CALCulate:WAVeform:MARKer:CPSearch[:STATe] <bool>

(Read-Write) Sets and read the Continuous Peak Search. Enables or disables the Continuous Peak Search. When Continuous Peak Search is on, a peak search is automatically performed for the selected marker after each sweep. The rules for finding the peak are exactly the same as for Peak Search, including the use of peak criteria rules.

Relevant Modes

IQA  (Waveform Only)

Parameters

 

<boolean>

ON (1) - Enables continuos peak search.

OFF (0) - Disables continuos peak search.

Couplings

N/A

Examples

CALC:WAV:MARK:CPS ON

CALC:WAV:MARK:CPS 0

Query Syntax

CALC:WAV:MARK:CPS?

Default

OFF (0)


Last Modified:

22oct2017

New IQA mode (10.1x)