(Read-Write) Set and read the automatic interval span setting for the selected I/Q marker. |
|
Relevant Modes |
IQA (Waveform only) |
Parameters |
|
<bool> |
Band power frequency span method. ON (or 1) - Interval Power frequency span is 5% (default) of existing frequency span (Stop Time - Start Time). OFF (or 0) - Set Interval Power frequency span manually using CALCulate:WAVeform:MARKer:FUNCtion:INTerval:SPAN |
Examples |
CALC:WAV:MARK:FUNC:INT:SPAN:AUTO 1 |
Query Syntax |
CALCulate:WAVeform:MARKer:FUNCtion:INT:SPAN:AUTO? |
Default |
ON |
Last Modified:
22oct2017 |
New IQA mode (10.1x) |