CALCulate[:SELected]:MARKer<n>:FUNCtion:PLEFt

(Write-Only) Causes the specified marker to find the next data point to the left that meets the 'Peak' criteria. When no data points to the left meet the Peak criteria, the marker does not move.

Relevant Modes

NF, PAA, SA, RTSA

Note: SA & RTSA modes do NOT recognize the optional [:SELected] node.

Parameters

 

<n>

New or existing marker to move. Choose from 1 to 6.

Examples

CALC:MARK1:FUNC:PLEF

Query Syntax

Not Applicable

Default

Not Applicable


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)

10-june-2016

Added RTSA mode (9.50)