(Read-Only) Reads the Y-axis uncertainty value for the specified marker. This command operates on the selected trace. First select a trace using CALC:PAR<tr>:SELect. |
|
Relevant Modes |
NF - One value is returned for symmetric values (Noise Factor and Noise Temperature) and two values are returned for asymmetric values (Noise Figure). |
Parameters |
|
<n> |
Existing marker for which to read Y-axis value. Choose from 1 to 2. |
Examples |
CALC:MARK1:Y:UNC? |
Return Type |
Numeric |
Default |
Not Applicable |
Last Modified:
01june2018 |
Added NF mode Opt. 356 (10.3) |