|
(Write) Add a comma separated list that contains the following: center frequency (CF), frequency span (span), and integrated bandwidth (iBW) |
|
|
Relevant Modes |
Channel Scanner |
|
Parameters |
|
|
<List> |
Choose from:
Caution: IMPORTANT! At this time the span argument is ignored in the FieldFox.
|
|
Examples |
:CHSCanner:EDIT:LIST:ADD 1e9,10e6,3e6 'set center frequency to 1 GHz, span to 10 MHz, and the integrated bandwidth to 3 MHz Caution: IMPORTANT! At this time the span argument is ignored in the FieldFox (e.g., in the example shown above the 10e6 span value is ignored). |
|
Query Syntax |
N/A |
|
Return Type |
Comma-separated numeric list |
|
Default |
Not Applicable |
Last Modified:
|
01nov2019 |
Added a Caution to this command |