|
(Read-Write) Set and query the number of traces to include in the large marker display state. |
|
|
Relevant Modes |
NA |
|
Parameters |
|
|
<x> |
Display state. Choose from: A - Display state A B - Display state B |
|
<char> |
Trace configuration. Choose from: D1 - One trace. D2 - Two traces overlaid on one graticule. D3 - Three traces overlaid on one graticule. |
|
Examples |
DISP:MARK:LARG:B:TRAC:COUN D3 |
|
Query Syntax |
DISPlay:MARKer:LARGe:<x>:TRACe:COUNt? |
|
Return Type |
Character |
|
Default |
D1 |
Last Modified:
|
22-Sept-2014 |
New command |