(Read-Write) Set and query the trace data type (Bar Chart and Strip Chart only). NOTE: Only one trace data type result can be displayed. Choice decides which data type is shown on GUI. |
|
Relevant Modes |
|
Parameters |
|
<string> |
Choices: DMRS: Demodulation Reference Signal RSRP: Reference Symbol Received Power RSRQ: Reference Signal Received Quality RSSI: Reference Signal Strength Indicator PBCH: Physical Broadcast Channel) EVM (%rms) PSS: The power level in dB for the primary synchronization signal, relative to the average subcarrier power. SSS: The power level in dB for the secondary synchronization signal, relative to the average subcarrier power. POWer: Channel power |
Examples |
DISP:NREVm:TRACe:DATA SINR DISP:NREVm:TRACe:DATA PSS |
Query Syntax |
DISP:NREVm:TRACe:DATA? |
Return Type |
string |
Default |
RSRP |
Last Modified:
22-044-2026 |
New command |