ffSDISPlay:NREVm:TRACe:DDATa <character>

(Read-Write) Set and query the demodulated IQ data signal displayed.

NOTE: This setting is only relevant to the constellation display and applies to all such displays (it cannot be set individually for each display).

NOTE: Only one trace data type result can be displayed. Choice decides which data type is shown on GUI.

Relevant Modes

5G NR EVM Conducted

Parameters

 

<char>

The signal demodulated IQ data displayed. Choose from:

ALL – Display the demodulated IQ data for all signals (PSS, SSS, PBCH and PBCH DMRS)

PSS – Display the demodulated IQ data for the PSS signal.

SSS – Display the demodulated IQ data for the SSS signal.

PBCH – Display the demodulated IQ data for the PBCH signal.

PBCHDMRS – Display the demodulated IQ data for the PBCH DMRS signal

Examples

DISP:NREVm:TRACe:DDATa PBCH

DISP:NREVm:TRACe:DDATa PSS

Query Syntax

DISP:NREVm:TRACe:DDATa?

Return Type

character

Default

ALL


Last Modified:

22-044-2026

New command