DISPlay:NREVm:WINDow[:SELect] <int>

(Read-Write) Set and query the selected window.

Relevant Modes

NREVm

Parameters

 

<integer>

Choices: 1 through 4. (Up to four windows can be selected/active at one time on the FieldFox.)

Examples

DISP:NREVm:WIND 2

Query Syntax

DISP:NREVm:WIND?

Return Type

numeric

Default

1


Last Modified:

22-044-2026

New command for 5G NR (11.5x)