DISPlay:NREV:WINDow<n>:BCHart:CCODing <char>

(Read-Write) Set and query the bar chart display color coding scheme.

Relevant Modes

5G NR EVM Conducted

Parameters

 

<n>

Window number. If unspecified, value is set to 1.

n = 1 | 2 | 3 | 4  (Up to four windows can be selected/active one time on the FieldFox.)

<char>

Choices:

Component Carrier (CC): Magnitude spectrum frequency domain (fixed span). You can only view a single component carrier at a time with Spectrum (e.g., CC0 or CC2, etcetera).

LEVel (LEV): Cell scan numeric results (for up to 6 cell sites (ID's) including Physical Channel Information (PCI) – (Cell ID), RSRP, RSRQ, RSSI, PSS, SSS, SINR, Freq Err.

PCI (PCI): Vertical power bar graph of selectable cell scan result metric for up to 6 cell sites with adjustable color "heat" amplitude scale

Couplings:

 

- This setting is associated with the currently selected window.

- This setting is only relevant for the bar chart display.

- When Level is selected, you can set the red and blue limits in the Scale/Amptd menu.

Examples

DISP:NREV:WIND2:BCH:CCOD CC */associates the selected component carrier with each bar

DISP:NREV:WIND4:BCH:CCOD PCI */associates the selected PCI with each bar

DISP:NREV:WIND4:BCH:CCOD PCI */associates the level of the value associated with each bar

Query Syntax

DISP:NREV:WIND3:BCH:CCOD?

Return Type

character

Default

LEVel


Last Modified:

22-044-2026

A12.00 New command