(Read-Write) Set and query the selected window data. |
|
Relevant Modes |
|
Parameters |
|
<n> |
Window number. If unspecified, value is set to 1. n = 1 | 2 | 3 | 4 (Up to four windows can be selected/active one time on the FieldFox.) |
<string> |
Choices: TABLe (TAB): Cell scan numeric results (for up to 6 cell sites (ID's) including Physical Channel Information (PCI) – (Cell ID), PSS, SSS, Channel Power, Sync Correlation Threshold. Bar CHart (BCH): Vertical power bar graph of selectable cell scan result metric for up to 6 cell sites with adjustable color "heat" amplitude scale SPECtrum (SPEC): Magnitude spectrum frequency domain (fixed span). You can only view a single component carrier at a time with Spectrum (e.g., CC0 or CC2, etcetera). Strip CHart (SCH): Magnitude of selectable cell scan result metric graphed over time. Couplings: Strip Chart should be active in only one window. If the strip chart window is disabled, it can be re-enabled in another active window. When the strip chart window is re-enabled, trace data is automatically reset to Table. CONStellation - Constellation diagram of the demodulated IQ data associated with the selected signal(s). FRAMe - Table of the frame summary results for the measured signals. |
Examples |
DISP:NREVm:WIND2:DATA BCH DISP:NREVm:WIND4:DATA SPEC |
Query Syntax |
DISP:NREVm:WIND3:DATA? |
Return Type |
string |
Default |
TABL |
Last Modified:
22-044-2026 |
New command |