:DISPlay:TABLe:MARKer:WAVeform <bool>

(Read-Write) Set or read the marker table. Enables the marker table to display below the graph on the FieldFox.

Relevant Modes

IQA (Waveform Only)

Parameters

 

<boolean>

Band power frequency span method.

ON (or 1) - Enables the marker table below the graph that displays the status of all six of the waveform markers.

OFF (or 0) - Disables the displayed marker table.

Couplings

If marker table is enabled, the marker table is only displayed when the active window number is 1.

Examples

DISP:TABL:MARK:WAV 1  

Query Syntax

DISP:TABL:MARK:WAV?

Return Type

Boolean

Default

OFF


Last Modified:

22oct2017

New IQA mode (10.1x)