DISPlay:TIME:FMT <char>

(Read-Write)  Set and query the format of the system time on the screen. Set the time using SYST:TIME

Relevant Modes

ALL

Parameters

 

<char>

System time format. Choose from:

Argument - Example

HIDE - time is not shown on screen.

SHORT - 10:31 PM

LONG - 10:31:25 PM

SH24 - 22:31

LO24 - 22:31:25

Examples

DISP:TIME:FMT Long

Query Syntax

DISPlay:TIME:FMT?

Return Type

Character

Default

Long