DISPlay:WINDow:TRACe<n>:STATe <bool>

(Read-Write) Set and query the display state of the data trace. To display both data and memory, set both to ON.  DISPlay:WINDow:TRACe<n>:MEMory[:STATe] sets the memory trace ON.

For NF mode, see also DISP:WIND:TRAC<n>:STOR.

Relevant Modes

CAT, NA, NF

Parameters

 

<n>

Trace number. If unspecified, value is set to 1.

For CAT mode Choose from 1 to 2.

For NA mode Choose from 1 to 4.

<bool>

Choose from:

O or OFF - Data trace NOT displayed

1 or ON - Data trace displayed

Examples

DISPlay:WINDow:TRAC1:STAT 1

Query Syntax

DISPlay:WINDow:TRACe2:STATe?

Default

1 -Displayed


Last Modified:

01june2018

Added NF mode Opt. 356 (10.3)

26-Apr-2012

Modified for CAT (5.75)