These commands are used for memory storage and retrieval.
See also MMEM:DATA.
|
Note: If you attempt to save a filename that has already been saved at the specified memory location, the FieldFox displays the following error message: Error -257, File name error; Storage Path "[INTERNAL]:\my_file" is not allowed. |
|
:MMEMory:DATA "<file_name>",#ABC This command writes <data> into "<file_name>", where <data> is in 488.2 block format. The FieldFox expects to see waveform data as block data (binary files). The IEEE standard 488.2-1992 section 7.7.6 defines block data. The following example shows how to structure a SCPI command for downloading waveform data where #ABC represents the block data.
|
|
|
|
Note: The following commands are not supported for non-volatile waveform memory (NVWFM). |
|
:MMEMory:CATalog? "<file_system>" This query outputs a list of the files from the specified file system. The return data will be in the following form: <mem_used>,<mem_free>{,"<file_listing>"}.
:MMEMory:CDIRectory "[<directory_name>]", "[<directory_name>]" :MMEMory:CDIRectory? This command changes the directory name for a file system. If no parameter is specified, the directory is set to the *RST value. At *RST, this value is set to the default user data directory. The query returns the full path of the default directory.
:MMEMory:COPY "<file_name>","<file_name>" This command makes a duplicate of the requested file.
:MMEMory:DELete "<file_name>",<directory_name> This command removes a file from the specified directory.
:MMEMory:MDIRectory <directory_name> This command creates a new directory where the <directory name> parameter specifies the name of the new directory. :MMEMory:MOVE "<src_file>","<src_file_1>" This command renames the src_file to src_file_1. :MMEMory:RDIRectory <directory_name> This command removes a directory where the <directory_name> parameter specifies the name of the directory to be removed. All files and directories under the specified directory are also removed. |
Last Modified:
|
22sep2017 |
Added 10.00. |