The following IEEE 488.2 Common Commands can be used with the FieldFox:
Clears the instrument status byte by emptying the error queue and clearing all event registers. Also cancels any preceding *OPC command or query.
Sets bits in the standard event status enable register.
Returns the results of the standard event enable register. The register is cleared after reading it.
Reads and clears event status enable register.
Returns a string that uniquely identifies the FieldFox. The string is of the form "Keysight Technologies",<model number>,<serial number>,<software revision> and so forth.
Generates the OPC message in the standard event status register when all pending overlapped operations have been completed (for example, a sweep, or a Default).
Returns an ASCII "+1" when all pending overlapped operations have been completed.
Returns a string identifying the analyzer option configuration.
Executes a device reset and cancels any pending *OPC command or query. All trigger features in HOLD. The contents of the FieldFox non-volatile memory are not affected by this command.
Before reading a status register, bits must be enabled. This command enables bits in the service request register. The current setting is saved in non-volatile memory.
Reads the current state of the service request enable register. The register is cleared after reading it.
Prohibits the instrument from executing any new commands until all pending overlapped commands have been completed.