(Read-Write) Set and query the status of the remote SCPI lockout (ON (1) or OFF (0)). See also, SYST:PRES. |
|
Relevant Modes |
ALL |
Parameters |
|
<bool> |
Choose from: O
or OFF - Remote lockout
is off.
Sending another SCPI command will turn on
the remote lockout feature
and an 1 or ON - Remote lockout is on.Sending another SCPI command will turn off remote lockout feature . Nothing is displayed at the top center of the FieldFox display. |
Examples |
INST:RLOC:DIS 0 'Remote lockout is disabled. |
Query Syntax |
INST:RLOC:DIS? |
Return Type |
Boolean |
Default |
ON (1) |
Last Modified:
01dec2019 |
New command |