(Write-Only) Store a noise figure ENR (*.enr) file to the specified device.
Note: Template *.enr files for several common models of noise sources may be found in the default ENR table directory of the FieldFox. In these files, the reflection coefficients have been set to the values specified for the respective model numbers, but the values for the ENR or ENR uncertainty will need to be entered at each frequency. See also, MMEMory:LOAD:ENR. |
|
Relevant Modes |
|
Parameters |
|
<string> |
For *enr files, provide filename of the *enr file WITHOUT an extension. |
<char> |
Memory device where the ENR file is stored. Choose from the following:
|
Examples |
MMEM:STOR:ENR "MySNR",INT |
Query Syntax |
Not Applicable |
Default |
Not Applicable |
Last Modified:
01june2018 |
Added NF mode Opt. 356 (10.3) |