MMEMory:STORe:IQCapture:DEVice

(Read-Write) Set and query the type of device storage type for IQA data capture (i.e., INT, USB, or SD).

Use MMEM:STOR:IQC:FTYP to set the data capture file type.

Use MMEM:STOR:IQC:FCO to manually set the IQA file capture count.

Relevant Modes

IQA

Parameters

 

<"device">

Data capture device storage-type.

INT - internal FieldFox memory

SD - SD card

USB - USB storage device

Examples

MMEM:STOR:IQC:DEV SD

Query Syntax

MMEM:STOR:IQC:DEV?

Return Type

character

Default

INT


Last Modified:

22-Oct-2017

Added new IQA mode content (10.1x).