:RECPlayback:ACTion:TPOSition <num>

(Read-Write)  Set and return the current trace position.  Use this command to move to a specific trace recording number when playback is paused.

Relevant Modes

SA, RTSA

Parameters

 

<num>

Enter a value between 1 and the total number of recorded traces.

Examples

RECP:SESS:TPOS 2

Query Syntax

:RECPlayback:ACTion:TPOSition?

Default

Not Applicable


Last Modified:

10-june-2016

Added RTSA mode (9.50)