:RECPlayback:CONFig:PTINterval <num>

(Read-Write) Set and return the Playback Time Interval - the delay that occurs between each trace as it is played back.

Relevant Modes

SA, RTSA

Parameters

 

<num>

Playback Time Interval (in seconds). Choose a delay value between 0 (play as fast as possible) and 100.

Examples

RECP:CONF:PTIN 10

Query Syntax

:RECPlayback:CONFig:PTINterval?

Default

0


Last Modified:

10-june-2016

Added RTSA mode (9.50)