(Read-Write) Set and return the Record Segment Counting Length - the number of traces to record, after which the recording will automatically pause. Use Pause/Resume or Record to capture another <num> traces, or Stop to end recording. When set, a counter appears in the lower-left corner which counts UP to the specified number of recordings. |
|
Relevant Modes |
SA, RTSA |
Parameters |
|
<num> |
Number of traces to record. Choose a value between 0 (no limit to the number of traces) and 100. |
Examples |
RECP:CONF:RSCL 10 |
Query Syntax |
:RECPlayback:CONFig:RSCLength? |
Default |
OFF - NO limit to the number of traces to be recorded. |
Last Modified:
10-june-2016 |
Added RTSA mode (9.50) |