:RECPlayback:CONFig:RSOurce <char>

(Read-Write) Set and return the Record Source - the location in the FieldFox data flow from where data is recorded.

Relevant Modes

SA, RTSA

Parameters

 

<num>

Record Source. Choose from:

FATR - First Active Trace. Means the first active trace that is not set to BLANK and or not set to VIEW. (RTSA mode only)

RAWM - Records raw measurement data (SA mode only)

TRA1 - Trace 1

TRA2 - Trace 2

TRA3 - Trace 3

TRA4 - Trace 4

Examples

RECP:CONF:RSO RAWM

Query Syntax

:RECPlayback:CONFig:RSOurce?

Default

FATR (RTSA mode default)

RAWM (SA mode default)


Last Modified:

10-june-2016

Added RTSA mode (9.50)