:RECPlayback:CONFig:RTLSeconds <num>

(Read-Write) Set and return the Record Time limit seconds - the time duration for the recording,  after which the recording will automatically pause. Use Pause/Resume to capture another <num> seconds, or Stop to end recording.

When set, a timer appears in the lower-left corner which counts DOWN from the specified number of seconds.

Relevant Modes

SA, RTSA

Parameters

 

<numeric>

Record Time limit (in seconds). Choose a delay value between 0 (NO limit -MAX) and 1e6 seconds.

Examples

RECP:CONF:PTLS 100

Query Syntax

:RECPlayback:CONFig:RTLSeconds?

Default

0 - NO limit to the number of seconds for a recording.


Last Modified:

10-june-2016

Added RTSA mode (9.50)