:RECPlayback:SESSion:TRLimit <num>

(Read-Write) Trace record limit for the current record playback session (Opt 236). An upper limit is set when the session opens. You can reduce this value to save storage space, but you cannot increase it beyond the upper default limit.

Relevant Modes

SA, RTSA

Parameters

 

<numeric>

Trace record limit. Choose a value from 1 to the default upper limit. Send a query before setting this value to learn the upper limit.

Examples

RECP:SESS:TRL 100

Query Syntax

RECPlayback:SESSion:TRLimit?

Default

Not Applicable


Last Modified:

10-june-2016

Added RTSA mode (9.50)