(Read-Write) Sets the acquisition time between Density and Real-Time traces to AUTO. (Spectrogram is not supported.) |
|
Relevant Modes |
RTSA |
Parameters |
|
<Boolean> |
Automatically sets the range: 20 ms (2.00E-02) to 541.2 ms (5.412E-1) ON (1) - The FieldFox automatically sets the acquisition time. OFF (0) - Auto acquisition is disabled. |
Examples |
ACQ:TIME:AUTO |
Query Syntax |
[:SENSe]:ACQuisition:TIME:AUTO? |
Return Type |
numeric |
Default |
0 |
Last Modified:
19-sep-2016 |
Added new RTSA command (A.09.50). |