[:SENSe]:ADEMod:METRics:MMENable

(Read-Write) Enable or disable Peak+ and Peak- for all of the analog demodulation types in the demodulation window.

Relevant Modes

SA

Parameters

ON (1) - Enables Peak+ and Peak-

OFF (0) - Disables Peak+ and Peak-

<string>

 

Examples

:ADEM:METR:MMEN ON

Query Syntax

:ADEM:METR:MMEN?

Return Type

String

Default

OFF


Last Modified:

16-Dec-2015

Added AM/FM Metrics (A.12.3x)