[:SENSe]:CHPower:TAASelect <char>

(Read-Write) Set and query the USB triaxial antenna settings.

Note: SA mode must be set to measure Channel Power to use this command.

Relevant Modes

5G EVM

Couplings

None

Parameters

 

<character>

<character> Triaxial antenna axis choice. Choose from:

OFF – No axis control selected.

SALL – Sums all axes.

AX - X axis selected.

AY - Y axis selected.

AX - Z axis selected.

Note: Only one USB triaxial antenna is compatible with the FieldFox.

Examples

CHP:TAAS SALL */Sums all of the axes.

CHP:TAAS AX */Selects the X axis.

Query Syntax

CHP:TAAS?

Return Type

Character

Default

OFF


Last Modified:

01dec2019

New command