|
(Write-Read) Specifies the type of CalReady calibrations that is performed when the FieldFox is Preset. |
|
|
Relevant Modes |
CAT, NA To Cal in VVM mode, perform a Cal in CAT or NA mode, then switch to VVM mode. |
|
Parameters |
|
|
<char> |
Choose from: TWOPort - Corrects all four S-parameters. Requires a forward and reverse sweep, which causes slower trace measurements. ERESponse - (Enhanced response) Corrects forward (S21 and S11) and reverse (S12 and S22) measurements separately. Therefore, when measurements in only one direction are required, this choice provides faster trace measurements than a full 2-port cal. Note: There is no programming command to choose 'reciprocal' for Enhanced Response as there is from the User Interface. |
|
Examples |
CORR:COLL:CALR:TYPE TWOP |
|
Query Syntax |
[:SENSe]:CORRection:CALReady:TYPE? |
|
Default |
TWOPort |
Last Modified:
|
18-Oct-2012 |
New command |