|
(Write-Read) Set and query the state of the Omit Isolation setting. The optional isolation step of a calibration corrects for crosstalk which is the internal signal leakage between the test ports. The additional Isolation step measures Load standards that are connected to both FieldFox test ports. Perform an isolation calibration when you are testing a device with high insertion loss, such as the stop band of a filter or a switch in the open position. See FieldFox User's Guide for more information. |
|
|
Relevant Modes |
CAT, NA To Cal in VVM mode, perform a Cal in CAT or NA mode, then switch to VVM mode. |
|
Parameters |
|
|
<bool> |
Choose from the following: ON or 1 - Omit the Isolation step. OFF or 0 - Perform the Isolation step |
|
Examples |
CORR:COLL:OIS 1 Sense:Correction:Collect:Oisolation off |
|
Query Syntax |
[:SENSe]:CORRection:COLLect:OISolation? |
|
Default |
ON or 1 |
Last Modified:
|
1-Nov-2013 |
New command |