|
(Read-Write) Set and query the port extension ON | OFF state. Use [:SENSe]:CORRection:EXTension:PORT1 and [:SENSe]:CORRection:EXTension:PORT2 to set port extensions value. Use [:SENSe]:CORRection:RVELocity:COAX to set velocity factor. |
|
|
Relevant Modes |
CAT, NA |
|
Parameters |
|
|
<bool> |
Port extensions state. Choose from: 0 or OFF - Port extensions OFF 1 or ON - Port extensions ON |
|
Examples |
CORR:EXT 1 |
|
Query Syntax |
[:SENSe]:CORRection:EXTension[:STATe]? |
|
Return Type |
Boolean |
|
Default |
OFF |
Last Modified:
|
10-Aug-2010 |
New command (5.30) |