|
(Read-Write) Set and query the Blue Limit percent of the RTSA Mode Density trace display state. |
|
|
Relevant Modes |
RTSA |
|
Parameters |
|
|
<num> |
Set the Blue limit percentage to a value between 0.05 and 100. If you attempt to set the limit below 0.05, the instrument's blue limit will be set to 0.05 percent. |
|
|
|
|
Examples |
DENS:BPL 10 'Sets the blue limit percent to 10 percent. DENS:BPL .05 'Sets the blue limit to its minimum (default) percent of 0.05. |
|
Query Syntax |
DENS:BPL? |
|
Return Type |
num |
|
Default |
5.0E-02 |
Last Modified:
|
19-sep-2016 |
Added new cmd for RTSA mode (A.09.50). |