[:SENSe]:DIF:BANDwidth <num>

(Read-Write) Set and query the digital IF bandwidth of the instrument. This parameter is closely related to the sample rate.

Relevant Modes

IQA

Parameters

 

<numeric>

Minimum: 1

Maximum: 10000000

Examples

DIF:BAND 1000

DIF:BAND 5 kHz

DIF:BAND 5e3

Query Syntax

:DIF:BAND?

Return Type

numeric

Default

10000000


Last Modified:

22oct2017

New IQA command (A.10.1x)