Note: This command is only available on B model FieldFoxes and requires Option B04 or B10.
|
(Read-Write) Set and query the IQA/RTSA mode narrow (10 MHz) or wideband (40 MHz or 100 MHz) IF path. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<string> |
IFPath. Choose from: AUTO (default) - The IF path selected will depend on the frequency span being measured. It will be narrow (10 MHz capable) for span ≤10 MHz and will be wide (40 MHz or 100 MHz - option dependent) for span >10 MHz. B10M - 10 MHz narrow IF Path is selected. B100M - 40 MHz/100 MHz wide IF Path is selected (Option B04 or B10 required). |
|
Examples |
IFPath B100M */Selects the wide IF path, 40 MHz (Option B04) or 100 MHz (Option B10). IFPath AUTO */Default |
|
Query Syntax |
[:SENSe]:IFPath]? |
|
Return Type |
Character |
|
Default |
AUTO |
Last Modified:
|
|
New command |