[:SENSe]:MEASure

(Read-Write) Selects between Density, Spectrogram, and Real-Time traces.

Relevant Modes

RTSA

Parameters

 

<char>

Select the type of Real-Time measurement to be displayed:

DENSity - Signal is displayed is a real-time spectrum with a histogram bitmap.

SPECtrogram - The signal is displayed is a real-time spectrum with a spectrogram bitmap. Spectrogram views are valuable in capturing signals that include both time and frequency variations.

NORMal - The signal is displayed as a real-time spectrum. Use real-time spectrogram to quickly display measurements.

Examples

MEAS DENS

Query Syntax

[:SENSe]:MEASure?

Return Type

Character

Default

DENS


Last Modified:

19-sep-2016

Added  new RTSA command (A.09.50).