[:SENSe]:MEASure:SRATe <num>

(Read-Write) Set and query the IQA sample rate. The “Digital IF Bandwidth” parameter controls the resampler section of the hardware. It is directly coupled to the sample rate.

Sample Rate = (Digital IF Bandwidth) * (Over Sample Ratio)

                    = (Digital IF Bandwidth) * 1.25

Relevant Modes

IQA

Parameters

 

<numeric>

Minimum: 12.5 Hz

Maximum:

A-Series FieldFox: 12.5 MHz

B-Series FieldFox: 125 MHz

Couplings: (1.25 * IF Bandwidth)

Examples

MEAS:SRAT 1 MHz

MEAS:SRAT 10000

Query Syntax

MEAS:SRAT?

Return Type

Numeric

Default

1.250000000E+07


Last Modified:

06sept2019

Added B-Series 125 MHz BW.

22-Oct-2017

Added IQA mode (10.1x)