[:SENSe]:MEASurement:ADEMod (*NEW* BEHAVIOR - RECOMMENDED)

(Read-Write) Set the AM/FM Metrics measurement type (Select 1 of n measurement choices)

IMPORTANT! This topic describes the new behavior, which is recommended.

See also, ADEM:METR:DTYP and TAL:DTYP.

Relevant Modes

SA

Parameters

NONE - Turns off the AM/FM functionality.

TAL- Launch Tune & Listen mode

ADEM- Launch Analog Demod Metrics mode

<string>

 

Examples

:MEAS:ADEM NONE

Query Syntax

:MEAS:ADEM?

Return Type

String

Default

NONE


Last Modified:

16-Dec-2015

Added AM/FM Metrics (8.15 & 9.15)