(Read-Write) Set and query the Tune and Listen demodulation type for SA Mode. Note: This command has been obsoleted and is not completely compatible with current commands and features. It is strongly recommended that you use: ADEM:METR:DTYP. |
|
Relevant Modes |
SA |
Parameters |
|
<char> |
Tune and Listen demodulation type. Choose from: AM - AM FMN - FM Narrow FMW - FM Wide NONE - Tune and Listen OFF. |
Examples |
MEAS:TAL FMW *Sets Tune and Listen to FM Wide |
Query Syntax |
[:SENSe]:MEAS:TAListen? |
Return Type |
Character |
Default |
NONE |
Last Modified:
01july2021 |
Modified to be Obsolete command (A.12.3x) |
16-Dec-2015 |
Added AM/FM Metrics (8.15 & 9.15) |