|
(Read-Write) Set and query the frequency band and bandwidth value. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<char> |
Frequency band and bandwidth value. Choose from: FR15M – FR1 5 MHz bandwidth. FR110M - FR1 10 MHz bandwidth. FR115M - FR1 15 MHz bandwidth. FR120M - FR1 20 MHz bandwidth. FR125M - FR1 25 MHz bandwidth. FR130M - FR1 30 MHz bandwidth. FR140M - FR1 40 MHz bandwidth. FR150M - FR1 50 MHz bandwidth. FR160M - FR1 60 MHz bandwidth. FR170M - FR1 70 MHz bandwidth. FR180M - FR1 80 MHz bandwidth. FR190M - FR1 90 MHz bandwidth. FR1100M - FR1 100 MHz bandwidth. FR250M - FR2 50 MHz bandwidth. FR2100M - FR2 100 MHz bandwidth. |
|
Examples |
NREV:BAND FR110M */sets the bandwidth to FR1 5 MHz bandwidth NREV:BAND FR250M */sets the bandwidth to FR2 50 MHz bandwidth |
|
Query Syntax |
NREV:BAND? */queries the bandwidth value |
|
Return Type |
Character |
|
Default |
FR110M |
Last modified:
|
01-june-2018 |
New command |