|
(Read-Write) Set and query the operating band for the Component Carrier (CC). See 5G NR User Equipment (UE) radio transmission and reception; Part 1: Range 1 Standalone (3GPP TS 38.101-1 version 15.7.0 Release 15) Section 5.2 and 5G NR User Equiptment (UE) radio transmission and reception; Part 2: Range 2 Standalone (3GPP TS 38.101-2 version 15.7.0 Release 15) Section 5.2. |
|
|
Relevant Modes |
|
|
Couplings |
This setting is associated with the currently selected Component Carrier (CC). When a band other than None is selected, the Channel Raster & Sync Raster values are limited by the band. The SCS setting is coupled with the Band (only certain bands are available for each SCS). |
|
Parameters |
|
|
<n> |
Component carrier (CC) number. If unspecified, value is set to 1 (CC0). n = 1 | 2 | 3 | 4 | 5 |
|
<char> |
The frequency mode. Choose from: NONe: No band The Nx operating band values: n1 | n2 | n3 | n5 | n7 | n8 | n12 | n20 | n25 | n28 | n34 | n38 | n39 | n40 | n41 | n50 | n51 | n66 | n70 | n71 |
|
Examples |
NREV:CCAR5:BAND N50 */Sets the operating band N50 for the CC4 NREV:CCAR3:BAND NON */Sets the operating band NONE for the CC2 |
|
Query Syntax |
NREV:CCAR<n>:BAND? */queries the operating band for specified CC |
|
Return Type |
character |
|
Default |
<n> =1, <character> = NON |
Last Modified:
|
10jun2024 |
New command |