|
(Read-Write) Set and query the component carrier's enable/disable state. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<n> |
Component carrier (CC) number. If unspecified, value is set to 1 (CC0). n = 1 | 2 | 3 | 4 | 5 (Up to five component carriers can be measured at one time.) |
|
<bool> |
Choices: ON (1): Enables the current component carrier. OFF (0): Disables the current component carrier. |
|
Examples |
NREV:CCAR5:ENAB ON NREV:CCAR3:ENAB 0 |
|
Query Syntax |
NREV:CCAR:ENAB? |
|
Return Type |
boolean |
|
Default |
ON for CC0. OFF for all other CC. |
Last Modified:
|
12dec2019 |
New command |