|
(Read-Write) Set and query the raster mode for the Component Carrier (CC). See 5G NR User Equipment (UE) radio transmission and reception; Part 1: Range 1 Standalone (3GPP TS 38.101-1 version 15.7.0 Release 15) Section 5.4.2 and 5.4.3 and 5G NR User Equipment (UE) radio transmission and reception; Part 2: Range 2 Standalone (3GPP TS 38.101-2 version 15.7.0 Release 15) Section 5.4.2 and 5.4.3. |
|
|
Relevant Modes |
|
|
Couplings |
This setting is associated with the currently selected Component Carrier (CC). The setting is only relevant when the Freq Mode is set to Channel. When Channel is selected, the Channel Raster settings are used to set the frequency settings and when Synchronization is selected, the Synchronization Raster settings are used to set the frequency settings. |
|
Parameters |
|
|
<n> |
Component carrier (CC) number. If unspecified, value is set to 1 (CC0). n = 1 | 2 | 3 | 4 | 5 |
|
<char> |
The raster mode. Choose from: CHANnel - Use the Channel Raster setting to set the frequency setting. SYNChronization - Use the Synchronization Raster setting to set the frequency setting. |
|
Examples |
NREV:CCAR:RMOD SYNC */Sets the raster mode to synchronization for CC0 NREV:CCAR3:RMOD CHAN */Sets the raster mode to channel for CC2 |
|
Query Syntax |
NREV:CCAR<n>:RMOD? */queries the raster mode for specified CC |
|
Return Type |
character |
|
Default |
<n> =1, <character> = CHAN |
Last Modified:
|
10jun2024 |
New command |