|
(Read-Write) Set and query the auto Cell ID value. Set the Cell ID using [:SENSe]:NREVm:CID:AUTO. |
|
|
Relevant Modes |
|
|
Parameters |
|
|
<char/num> |
Set the Cell ID. Choose from: <num> - Cell ID value. Choose a value between 0 and 1007. MINimum - Sets the Cell ID to the minimum value (0). MAXimum - Sets the Cell ID to the maximum value (1007). This command will accept MINimum and MAXimum as arguments. |
|
Couplings> |
Can only be set when [:SENSe]:NREVm:CID:AUTO Cell ID is OFF. |
|
Examples |
NREV:CID MIN */Sets the Cell ID to the minimum cell ID NREV:CID 505 */Sets the Cell ID to 505 |
|
Query Syntax |
NREV:CID? */queries Cell ID |
|
Return Type |
Numeric |
|
Default |
ON (1) |
Last Modified:
|
01dec2019 |
New command |