|
(Read-Write) Set and query the export Component Carrier (CC). The results of the selected CC are exported to the measurement setup of the corresponding CC in the 5G NR submode with the [:SENSe]:NREVm:RESults:EXPort command. |
|
|
Relevant Modes |
|
|
Couplings |
This setting is associated with the currently selected Component Carrier (CC). This setting is limited by the Band setting. The Channel ARFCN is translated to a frequency and used to set the Center Frequency setting. |
|
Parameters |
|
|
<char> |
Component carrier (CC) value. Choose from: CC0 – Component Carrier 0. CC1 – Component Carrier 1. CC2 – Component Carrier 2. CC3 – Component Carrier 3. CC4 – Component Carrier 4. |
|
Examples |
NREV:RES:EXP:CCAR CC4 |
|
Query Syntax |
NREV:RES:EXP:CCAR? |
|
Return Type |
character |
|
Default |
CC0 |
Last Modified:
|
01dec2019 |
New command |